{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Will GV2AF4 work with ATV320 instead of GV2AF5?
Issue:
Can I use GV2AF4 instead of GV2AF5 with ATV320 VFD?

Product Line:
ATV320

Environment:
All

Cause:
NA

Resolution:
GV2AF5 is a specific version of GV2AF4 aimed at better securing the assembly of an ATV320 below the GV2.

In some cases, GV2AF4 would pop out of ATV320 screw terminals.
GV2AF5 is slightly different as compared to GV2AF4. In addition, it has a kind of specific hook at the bottom rear part in order to properly secure the ATV320 to GV2AF5.
Connection is possible with GV2AF4 + VW3A9921, but pressure needs to be applied on GV2 to secure a good connection.

The final solution is to use the new part GV2AF5.