{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why cannot see the appliance disconnected in the GateManager of Ecostruxure Secure Connect Advisor?
In Ecostruxure Secure Connect Advisor, in the Tab "Audit" of the GateManager, there is the possibility is see when the appliance is connected.
However, only the status "Appliance Connect" is visible. The status "Appliance disconnect" is not reported in the history
In the following screenshot, only "Connect" is visible
Gatemanager view1

This Article is applicable for Ecostruxure Secure Connect Advisor

If the use want to be informed when the appliance is disconnected, there is a possibility using Alert function
In order to create the Alert function, need to have a GateManager Premium Access (ref: VJOCNTGMPREM)

Then right click on Domain name, and select "create alert"
Gatemanager view2

Select the appliance
Gatemanager view3

Result
email result



Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.