Issue
In Vijeo Designer, how do I set my driver settings in order for my HMI to communicate with a BMENOC0321 module for Modicon M580 via the Modbus TCPIP protocol?
Product Line
Vijeo Designer, Modicon BMENOC0321 X80 Ethernet communication module
Environment
HMI Configuration software for Windows PC
Resolution
In Vijeo Designer,
1) In the Project Navigator window, right-click on the IO Manager node
2) Choose "New Driver…", this will open the New Driver dialog
3) From the Manufacturer dropdown list, select "Schneider Electric Industries SAS"
4) Choose the Driver "Modbus TCP/IP"
5) Choose the Equipment "Modbus Equipment"
6) Click OK
7) In the "Equipment Configuration" dialog, enter the IP Address of the BMENOC0321
8) Set the Unit ID (Modbus Node Equipment Address) to be 1 instead of the default 255
9) Tick the "IEC61131 Syntax" checkbox to use %M, %MW notation for the Device Addresses on variables
10) Under Variables -> Double Word word order, choose "Low word first"
When completed, the Equipment Configuration dialog should appear as follows (highlighted settings must be changed from default as per above steps):
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Global