{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
PSO Notification Settings and Notification History popup does not open
Issue
Where

Product Line
Power SCADA Operation 9.x

Environment
Power SCADA Operation 9.x

Cause
Known issue with PSO 9.0 CU2. Will be fixed in CU3

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

IMPORTANT: Solution is only applicable to Cumulative Update 2, do not apply if you are not updated to this version.

Find & Edit the "PLSNotification.ci" inside your PLS_Inlcudes project. Preferably using your Cicode Editor from your PSO Studio IDE.

Use the "Find Function" feature to find the following function:

```

LaunchNotificationSettings()

```

Inside this function there is a method/ subroutine called

```

DllClassCallMethod(m_oNotificationServiceInstance, "LaunchSettings", sDataPath, sIPs, sUserName, sLanguage);

```

Comment out the "sLangauge" argument & Re-terminate the statement. Like this.

```

DllClassCallMethod(m_oNotificationServiceInstance, "LaunchSettings", sDataPath, sIPs, sUserName);//, sLanguage);

```

Do the same for this FUNCTION:

LaunchNotificationHistory(STRING sFilter, STRING sClusterName = "")

Replace

```

DllClassCallMethod(m_oNotificationServiceInstance, "LaunchResults", sDataPath, sIPs, sClusterName, sFilter, sLanguage);

```

With

```

DllClassCallMethod(m_oNotificationServiceInstance, "LaunchResults", sDataPath, sIPs, sClusterName, sFilter);//, sLanguage);

```

Save the LaunchNotificationSettings function.

Update Pages in citect gfx builder.
Always "Pack" databases on your projects
Recompile your project. Remember to perform a full recompile, not an incremental one.
Always run "Computer Setup Wizard".
Run your project.

Schneider Electric Global