Issue:
Customer asking if all Altivar Drives have DC Bus Terminals
Product line:
Altivar Drives
Environment:
all
Cause:
Would like to know if the Altivar Drives have DC Bus Terminals
Resolution:
The Altivar 320, 340 and 900 series have DC bus terminals which has the PA+ and PC- for the DC bus voltage. PO or PB or PBe terminals can be used, if needed, for a braking resistor, as shown in each drive's Installation Manual. The ATV600 Series PA+ and PC- terminals are strictly for measuring DC Bus voltage levels.
Customer asking if all Altivar Drives have DC Bus Terminals
Product line:
Altivar Drives
Environment:
all
Cause:
Would like to know if the Altivar Drives have DC Bus Terminals
Resolution:
The Altivar 320, 340 and 900 series have DC bus terminals which has the PA+ and PC- for the DC bus voltage. PO or PB or PBe terminals can be used, if needed, for a braking resistor, as shown in each drive's Installation Manual. The ATV600 Series PA+ and PC- terminals are strictly for measuring DC Bus voltage levels.
Released for:Schneider Electric Global