Issue
Customer wants to know how to determine if there is an IP address duplicated on the backplane port or on the control port of the BMENUA0100 module.
Product Line
BMENUA0100
Environment
Firmware 1.01.50
Resolution
The following corrections will be taken in consideration in the next release of the BMENUA0100 documentation.
Customer wants to know how to determine if there is an IP address duplicated on the backplane port or on the control port of the BMENUA0100 module.
Product Line
BMENUA0100
Environment
Firmware 1.01.50
Resolution
The following corrections will be taken in consideration in the next release of the BMENUA0100 documentation.
Released for:Schneider Electric Global