{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What does the [ION_Data]- MAINTENANCE-Job task do under Windows Task Scheduler?
Issue
What does the [ION_Data]- MAINTENANCE-Job task do under Windows Task Scheduler?

Product Line
PME 7.x.x

PME8.x
PME9.x
PME2020

Environment
PME Software


Resolution


The ION_Data Maintenance job runs a powershell script which performs a defragmentation on ION_Data.  Details of the script can be found in
Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\cfg\DbScheduledTasks

Note: For large databases the function can take a long time to run which can slow down data insertion so at times it would be disabled to avoid this issue.