Issue
Definition of %SW117 listed for the PLC_STAT word 4 of the PLCSTAT DFB cannot be found in the help.
Product Line
Control Expert 14.1
Environment
Windows 10
Resolution
The PLCSTAT DFB from the Extras folder of the Control Expert v14.1 DVD provides the ability to convert the Quantum STAT block to an
M580 PLC STATUS block.. Within the PLCSTAT DFB code, there is a word %SW117 listed for the PLC_STAT word 4. The help
does not provide a definition of the error codes returned by the Control Expert for word %SW117..
Word %SW117 is used for the RIO status. The following is a list of definitions for the error codes that can be returned by %SW117
RIO STATUS CODE
RIO_ERR_INIT_FAILED 0x0010
RIO_ERR_CRP_HOTSWAP 0x0020
RIO_ERR_DIAG_FAILED 0x0030
RIO_ERR_BAD_STATE 0x0040
RIO_ERR_WRONG_VERS 0x0050
RIO_ERR_BAD_TCOP 0x0060
RIO_ERR_CRP_COM_ERROR 0x0070
RIO_ERR_CRP_MODE 0x0080
RIO_ERR_CRP_TIMEOUT 0x0090
Definition of %SW117 listed for the PLC_STAT word 4 of the PLCSTAT DFB cannot be found in the help.
Product Line
Control Expert 14.1
Environment
Windows 10
Resolution
The PLCSTAT DFB from the Extras folder of the Control Expert v14.1 DVD provides the ability to convert the Quantum STAT block to an
M580 PLC STATUS block.. Within the PLCSTAT DFB code, there is a word %SW117 listed for the PLC_STAT word 4. The help
does not provide a definition of the error codes returned by the Control Expert for word %SW117..
Word %SW117 is used for the RIO status. The following is a list of definitions for the error codes that can be returned by %SW117
RIO STATUS CODE
RIO_ERR_INIT_FAILED 0x0010
RIO_ERR_CRP_HOTSWAP 0x0020
RIO_ERR_DIAG_FAILED 0x0030
RIO_ERR_BAD_STATE 0x0040
RIO_ERR_WRONG_VERS 0x0050
RIO_ERR_BAD_TCOP 0x0060
RIO_ERR_CRP_COM_ERROR 0x0070
RIO_ERR_CRP_MODE 0x0080
RIO_ERR_CRP_TIMEOUT 0x0090
Released for:Schneider Electric Global