{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is there any automated way to modify the parameter Sensor Alignment of the module BMXAMI0810?
Issue
Fill the field Alignment automatically

Product Line
M580

Environment
Control Expert

Resolution
Control Expert has DFB's that you can write/read parameters
I/O Module LocationI/O VisionFunction Block
Local RackTopological addressing/IODDTREAD_PARAM, WRITE_PARAM
DeviceDDTREAD_PARAM_MX, WRITE_PARAM_MX

Adjustment Parameter limitation
In M580 RIO, adjustment parameters cannot be changed from the PLC application during operation (no support of READ_PARAM, WRITE_PARAM, SAVE_PARAM, RESTORE_PARAM).