Issue:
Download over USB cable fails to start when using a Virtual Machine (VMware, Fusion, etc) running EcoStruxure Operator Terminal Expert
Product Line:
HMISTO, HMIGTU, HMIST, EcoStruxure Operator Terminal Expert
Resolution:
When running EcoStruxure Operator Terminal Expert in a Virtual Machine (VMWare, Fusion, etc), ensure to set the USB Compatibility to version 1.1 if you require to download to the HMI via USB cable. If you leave it at 3.0 or 2.0, the USB download will not start.
Download over USB cable fails to start when using a Virtual Machine (VMware, Fusion, etc) running EcoStruxure Operator Terminal Expert
Product Line:
HMISTO, HMIGTU, HMIST, EcoStruxure Operator Terminal Expert
Resolution:
When running EcoStruxure Operator Terminal Expert in a Virtual Machine (VMWare, Fusion, etc), ensure to set the USB Compatibility to version 1.1 if you require to download to the HMI via USB cable. If you leave it at 3.0 or 2.0, the USB download will not start.
Released for:Schneider Electric Global