Yes.
Altivar series, ATV320 drives in IP65/66 (ATV320...W or WS) are equipped by compact version of ATV320 inside. Communication card inserted to ATV320 via adapter VW3A3600 is possible as there is still space and so IP65/66 will be kept.
See page from ATV320 catalog regarding VW3A3600 adapter and communicaiton card inserted into ATV320...W/WS.
Altivar series, ATV320 drives in IP65/66 (ATV320...W or WS) are equipped by compact version of ATV320 inside. Communication card inserted to ATV320 via adapter VW3A3600 is possible as there is still space and so IP65/66 will be kept.
See page from ATV320 catalog regarding VW3A3600 adapter and communicaiton card inserted into ATV320...W/WS.
Released for:Schneider Electric Global