Issue:
Is the IP address retained in the VW3A3627 for the ATV320 drive?
Product Line:
Altivar ATV320
Environment:
All serial numbers, all model numbers
Cause:
Customer want to have a preprogram IP address on Profinet Communication module (VW3A3627) so he didn't have to program when installed into the drive.
Resolution:
No, you cannot preprogram the IP address for the Profinet Communication Module (VW3A3627) because the address is not retained in the Card.
Is the IP address retained in the VW3A3627 for the ATV320 drive?
Product Line:
Altivar ATV320
Environment:
All serial numbers, all model numbers
Cause:
Customer want to have a preprogram IP address on Profinet Communication module (VW3A3627) so he didn't have to program when installed into the drive.
Resolution:
No, you cannot preprogram the IP address for the Profinet Communication Module (VW3A3627) because the address is not retained in the Card.
Released for:Schneider Electric Global