Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
What is the correct 3.3V Power Budget for the BMXDRA0815 module?
Issue
The BMXDRA0815 modules 3.3V Power Budget is incorrect in Control Expert 14 and 14.1.
Product Line
M580
BMXDRA0815
Resolution
The correct 3.3V Power Budget for a BMXDRA0815 is 40ma.
It is incorrectly calculated and displayed as 100ma in CE14 and 14.1.
This issue is corrected in Control Expert version 15.
The BMXDRA0815 modules 3.3V Power Budget is incorrect in Control Expert 14 and 14.1.
Product Line
M580
BMXDRA0815
Resolution
The correct 3.3V Power Budget for a BMXDRA0815 is 40ma.
It is incorrectly calculated and displayed as 100ma in CE14 and 14.1.
This issue is corrected in Control Expert version 15.
Explore more
Range:
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}
Explore more
Range: