Issue
Unity14-UnityLL984 Library install returns ObjectStore error
Product Line
Control Expert 14
Environment
Windows 10
Resolution
Installingt the 'UnityLL984 Library' into Control Expert 14, returns the following ObjectStore error.

To resolve the issue:
Unity14-UnityLL984 Library install returns ObjectStore error
Product Line
Control Expert 14
Environment
Windows 10
Resolution
Installingt the 'UnityLL984 Library' into Control Expert 14, returns the following ObjectStore error.
To resolve the issue:
- Unzip and run the attached batch file named 'UpdateRegistry'.
- Install the 'UnityLL984 Library'.
Released for:Schneider Electric Global