Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

		
Search FAQs
Is BMXAMI0810 tolerant to HART signal?

Issue
Customers want to use the analog HART instruments with BMXAMI0810.

Product Line
x80 Modules

Environment
EcoStruxure Control Expert v14.0, BMEP584040, BMXAMI0810

Resolution
HART instruments have Digital and Analog signal with Frequency Shift Keying (FSK).
This is related to analog sampling. In most cases it doesn’t sample just exactly the full digital sinewave cycle or the multiples of it, then there’s the interference introduced. So, to be HART compliant it needs a HART signal filter on the input that currently the BMXAMI0810 does not have otherwise a maximum deviation within +/-0.5mA can be seen due to the HART FSK.
So, in case HART information is part of the signal to be measured, an ABE-7CPA31E interface sub-base has to be used in order to filter this information that would disrupt the analog value.

Schneider Electric also has the BMEAHI0812 that is an analog input module for specific for HART inputs.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Our Mission
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Financial Results
  • Annual Reports
  • Share Price
  • Investor Events
  • Careers
  • Sustainability
  • Electricity 4.0
  • Next-generation Automation
  • AI and Technology
  • Reports
  • Foundation
  • Consulting
  • Global - FR
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Change your cookie settings