1.Issue
Can the BMXERT1604T be synchronized without IRIG-B and DCF77 source in a M580 project ?2.Environment
M580 series
3.Resolution
The BMXERT1604T with Firmware version >=SV2.0 could be synchronized by M580 Standalone CPU via Xbus by selecting CPU/CRA head as externel clock source.
User needs to select BMXERT1604.2 during hardware configuration .
The clock sync source needs to be CPU/CRA head
Detailed compatibility matrix is shown as below
Released for:Schneider Electric Global