- Issue
Customer needs technical support on the configuration of BMXMSP0200 to control drive.
- Product Line
- Environment
- Resolution
1> Create a new application in Unity Pro or Control Expert.
2> Configurate the M340 and BMXMSP0200 in the hardware.
3> Set the parameter of BMXMSP0200.
4> Create the EFB instance as below snapshot indicates.
5> And then build change and transfer the application to the CPU.
6> After all, you can debug this demo application.
Released for:Schneider Electric Global