Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

		
Search FAQs
What are the rules to be followed for SPD mounting inside BlokSeT equipment?
Below are the rules which we need to follow for the SPD mounting inside BlokSeT.
  1. The surge arrester connections between the network (through the disconnection device) and the earth terminal block does not exceed 50 cm.
  2. 50cm rules of cable length is derived based on the inductance of the cable. So, the inductance of wire plays a major role to decide the cross section and length of cable.
  3. The length of cable can be increased to 1 m if the load connected to switchboard are of category 3 or 4 as per below table.
SPD - Overvoltage category
4. BlokSeT frame of the cubicle or other metallic parts can also be considered as earthing point for SPD, because all the metallic parts in the cubicles has earth continuity.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Our Mission
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Financial Results
  • Annual Reports
  • Share Price
  • Investor Events
  • Careers
  • Sustainability
  • Electricity 4.0
  • Next-generation Automation
  • AI and Technology
  • Reports
  • Foundation
  • Consulting
  • Global - FR
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Change your cookie settings