{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Custom RPI settings for the BMXCRA312x0 and the BMECRA312x0 Remote Adapters are not working when using Unity V13.1, CE V14 or V14.1.
Issue
Custom RPI settings for the BMXCRA312x0 and the BMECRA312x0 Remote Adapters does not work when using Unity V13.1, CE V14 or V14.1.
For example, if the RPI is set to 31 ms in the configuration,




But the RPI does not change to 31 ms in the DTM.



Note: This issue does not occur when configuring a 140CRA31200 Remote Adapter.


Product Line
M340
M580
BMXCRA31200
BMXCRA31210
BMECRA31210


Environment


Resolution
The issue is fixed in:
  • Control Expert 14.1 using HotFix 1 (HF1)
  • Control Expert 15.0



Schneider Electric Global