{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the replacement external reset button for Class 8536 Type SAG, Type SBG, or Type SCG starter?
Issue:
What is the replacement external overload reset button on the 8536 Type S starters?

Product line:
NEMA starter, 8536 Type SAG SBG SCG (, sizes 00, 0, 1)

Environment:
NEMA and Definite Purpose Contactors and Starters

Cause:
Replacement parts

Resolution:
Part number for the external reset bar/button is 9066SC1.

Schneider Electric Global

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: