Issue:
Video: Understanding the nLP Status on Altistart ATS48
Product Line:
Altistart ATS48
Cause:
No Mains voltage present on the input of the soft starter before start.
Resolution:
NLP means No Line Power. This indicates there is no mains power applied to the starter`s L1 - L2 - L3 terminals.
This may be due to a trip condition, but for a device with a line contactor, this is the normal off state.
,
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.