Issue:
Altistart 48 shorting contactor selection when also using for full voltage bypass.
Product Line:
Altistart 48 Soft Starters
Environment:
All
Cause:
NA
Resolution:
Yes. Shorting contactors are only rated for the AC1 rating. This means it is only rated to handle the continuous amps for the motor. It will be too small to handle the starting current. It is necessary to select full voltage bypass contactors based on the AC3 rating to handle the motor starting current.
It is also recommended to use external overload protection because the soft starter will not be able to provide the motor thermal protection when removed from the circuit for full voltage bypass.
CTA-ID : 7482
Altistart 48 shorting contactor selection when also using for full voltage bypass.
Product Line:
Altistart 48 Soft Starters
Environment:
All
Cause:
NA
Resolution:
Yes. Shorting contactors are only rated for the AC1 rating. This means it is only rated to handle the continuous amps for the motor. It will be too small to handle the starting current. It is necessary to select full voltage bypass contactors based on the AC3 rating to handle the motor starting current.
It is also recommended to use external overload protection because the soft starter will not be able to provide the motor thermal protection when removed from the circuit for full voltage bypass.
CTA-ID : 7482
Released for:Schneider Electric Global