Search FAQs

Are 21 volt replacement control coils available for LC2D4011?

Issue:
LC2D4011 replacement coil

Prodcut Line:
IEC Contactors and Starters

Product Line:
TeSys™ D Contactors

Resolution:
21VAC coils are not an option on these reversing change over contactors.
We do offer the B6 or B7 which is 24VAC.  The tolerance on the 24V coil is 85 to 110%.  So the 24VAC coil will work down to 20.4VAC.

Note the LC2D4011 series is obsolete.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Our Mission
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Financial Results
  • Annual Reports
  • Share Price
  • Investor Events
  • Sustainability
  • New Energy Landscape
  • Next-generation Automation
  • AI and Technology
  • Reports
  • Foundation
  • Consulting
  • Global - FR
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Change your cookie settings