{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Do we offer a 3-phase QO2175SB Surgebreaker?
Issue:
Is there a QO Surgebreaker that will work for 3-Phase, 208Y/120, 4-wire QO Load Centers?

Product Line:
Surge Protective Devices (SPD's)

Environment:
Installation

Resolution:
No, we do not. However, two QO2175SB Surgebreakers can be used in a QO 3-phase load center to protect a 208Y/120Vac, 3-phase, 4-wire system. To connect (2) QO2175SB units to a 208Y/120 panel, connect 1 unit to phases A & B and the other unit to phases B & C. In this case, the B phase will get double the surge current protection rating than phases A & C because it has both units connected to that one phase.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: