In case of a target such as HMIBMO HMIBMI is connected as equipment to a Site Manager such as HMIST6 or HMIBSC. The HMIBMI or HMIBMO is shows as "not connected", even if the target is correctly connected
This artible is applicable for EcoStruxure Secure Connect Advisor with HMIBMx using Windows 10 LTSB and LTSC
In order to shows the equiment connected, the windows firewall should allow the ping request. To do it, need to add a rules in the windows firewall to allow ICMPV4 (at least Echo Request)
This artible is applicable for EcoStruxure Secure Connect Advisor with HMIBMx using Windows 10 LTSB and LTSC
In order to shows the equiment connected, the windows firewall should allow the ping request. To do it, need to add a rules in the windows firewall to allow ICMPV4 (at least Echo Request)
Then just add the rule title to publish it And the HMIBMI / HMIBMO will be visible as equipment in your GateManager |
Released for:Schneider Electric Global