{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to do indirect addressing with the M221 in Machine Expert Basic.
Issue:
How to do indirect addressing with a M221.

Product Line:
M221

Environment:
Machine Expert Basic ( formally SoMachine Basic)


Causes and Fixes:
How to

Resolution:
1) open project
2) insert an operate block
3) Enter the following example %MW0[%MW10]:=200
4)  Create an Animation table
5) Enter in the following registers %MW0, %MW10, %MW5, and %MW15
6) Save and build changes
7) For this demo we will use the simulator in Machine Expert Basic to test
8) Load the project in simulator and place in RUN.
9) You will see a value of 200 in the %MW0
10) we will now go to %MW10 and put in the register that we want to move the data to we will enter the value of 5 and also 15 that will reference the %MW5 and %MW15 and it will move thedata of 200 to those registers.

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: