{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Vijeo Designer RunTime: What is the new registration policy from V6.2 SP11?
Vijeo Designer Licenses are now changing with the transformation of the Schneider Electric Registration Server. The goal of this article is to inform about the new registration policy.

This article is applicable to the following products:
HMIBM, Harmony P6, HMIG5U22, S-Panel PC, Third-Party PC

New registration policy:

Vijeo Designer RunTime: Starting with Vijeo Designer 6.2 SP11, it is strongly recommended to use the new PC RunTime Licenses (printed or mail), (Ref = VJDRPCCZLSPMZZ, VJDRPCCZLSPAZZ,  VJDHPCCZLSPMZZ, VJDHPCCZLSPAZZ) compatible with the current Schneider Electric Registration Server. On the targeted PC, you must install Vijeo Designer RunTime for Standard PC Version V6.2 SP11 from the folder “Runtime_For_Windows _SP11(6.2.11.22 _6.2.11.22)“                              Here is the link to download Runtime_For_Windows _SP11:
Runtime_For_Windows_SP11(6.2.11.23_6.2.11.23)


Here is the License Manager tool for Vijeo Designer Runtime 6.2 SP11

License Manager

Note: if you use any previous Vijeo Designer RunTime Licenses for iPC/PC ( Ref = VJDSNRTMPC, VJDSNRTSPC), you must first install on the PC a Vijeo Designer RunTime for Windows iPC/PC with version  V6.2 SP10 or lower version to register the license. Once you have done so, the Runtime PC  can be updated with the SP11 version.

Here is the link to download Runtime_For_Windows _SP10:
Runtime_For_Windows_SP10(6.2.10.23_6.2.10.21).7z

Schneider Electric Global

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: