{}

Welcome to the Schneider Electric corporate Website

Search FAQs
Why are HMISTU655 and HMISTU855 no more visible in the list of Target Models into Vijeo Designer 6.2 SP11?

Why are HMISTU655 and HMISTU855 no more visible in the list of Target Models into Vijeo Designer 6.2 SP11?

This FAQ concerns HMISTU655, HMISTU855, HMIS5T.

HMISTUx55s manufactured before 2012/03/12 (i.e. not marked with the label reference HMIS5T on the rear module) are no longer supported in VJD 6.2 SP11 and require a previous version of Vijeo Designer for their maintenance.

Summary:
-Labels with HMISTUx55 on rear module require Vijeo Designer 6.2 SP10 or less
HMISTU855

-Labels with HMIS5T on rear module can be used also with Vijeo Designer 6.2SP11 or moreHMIS5T

Schneider Electric Global

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range:
move-arrow-top