{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is Resi9 MP made of halogen free material?
Issue:
I want or need to use halogen-free Resi9 MP enclosures.

Product Line:
Resi9 MP

Cause:
Standard constraint

Resolution:
Yes, Resi9 MP is halogen-free except CR starting with MIP11 and MIP21 (because GWT850).

Notes:
To select the right enclosure, please select the product with the commercial reference starting with MIP10 / MIP12 / MIP 20 / MIP22.