{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Forbidden Architecture between BMENUA0100 and M580 CPU
The purpose of this note is to inform you about an architecture with BMENUA0100 and M580 HSBY CPU which can make problems in some cases.

In an HSBY Modicon M580 configuration, when the BMENUA0100 is connected to the same switch as the embedded Ethernet port of the M580 CPU, the OPCUA connection throughout the control port of BMENUA0100 could be lost after a swap or change-over of the M580 CPU.

To avoid this behavior, we recommend so to separate those networks.



Firmware version from 1.01 and above

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: