{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to use HMIPSPS752D1X01 COM2 for RS485 MODBUS RTU communication?

1.Please remove the HDD and check the DIP switch setting, we can refer to the information in the following picture.

The default setting of COM2 is RS-485/422.

2.After setting the DIP switch to RS485 mode, please enable "RS485 Auto Flow" in BIOS.

3.HMIPSPS752D1X01 is a product of Easy Line Harmony Panel iPC. The port definition of HMIPSPS752D1X01 is different with HMIPSP S-Panel PCs, so user can’t refer to the manual of HMIPSP S-Panel PCs.

Here is the Pin connection of HMIPSPS752D1X01 COM2, user can connect to Pin 3 and Pin7 for RS485 Modbus RTU communication.

Schneider Electric Global

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: