{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to interpret the information of the diagnosis indication ? Does it give the pole condition for all 3 poles ? What if the TeSys Giga contactor is only use 2 poles in the given application ? (Like to control single phase load/DC application).

Article available in these languages: Dutch

The indication is calculated globally, for all the 3 poles. If the application uses only 2 poles, we recommend removing the non-used pole (central one). Otherwise the wear diagnosis indication will not work.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: