Issue:
TA1 -TA4 parameters in the ATV61/ATV71 drives.
Product Line:
ATV61/ATV71 drives
Environment:
TA1- TA4 parameters
Cause:
n/a
Resolution:
TA1 (Rounding of the start of the ACC ramp) -Factory default is 10%
TA2 (Rounding of the end of the ACC ramp)-Factory default is 10%
TA3 (Rounding of the start of the DEC ramp)-Factory default is 10%
TA4 (Rounding of the end of the DEC ramp)-Factory default is 10%
Released for:Schneider Electric Global