{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the coil operating voltage and band / limit of different coils for TeSys Giga contactor ?
TeSys Giga have different variants of AC/DC wide band control voltage depending on the contactor type. The pick-up and drop-off voltage values are as below:
Advanced versionOperational limits
Pick-upDrop-off
24…48V AC/DC
48…130V AC/DC
200…500V AC/DC
0.8…1.1 Uc0.45 Uc
Standard version
48…130V AC/DC
100…250V AC/DC

Note that LC1G630…800 will launch in Q1 2022

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.