Issue:
Supported virtual environment for EcoStruxure Control Expert
Product Line:
EcoStruxure Control Expert
Resolution:
EcoStruxure Control Expert V15 SP1 has been successfully tested in the following virtual environment:
·VMware vSphere –Hypervisor- ESXi
·VMware Workstation 14 Pro 14.1.0
It has not been tested on Virtual Box 5.2.16-123759
Note: RAM memory of host computer should be 16GB if Control Expert is used in a Virtual machine with 8GB assigned to the Virtual machine.
Released for:Schneider Electric Global