{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is a Ot fault on a ATV212 drive?

Issue:

Getting Ot fault on a ATV212 drive

Product Line:

ATV212

Environment:

Ot faults

Cause:

n/a

Resolution:

This is a Overtorque fault. The calculated motor torque has reached the level set by Parameter F616 (Overtorque Detection Level)- factory default set to 130%, can increase, if needed.
F615 (Overtorque fault/alarm selection)- can set to 0 for Alarm or 1 for Fault.

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: