Issue:
Unable to log into features that require my username and password
Product Line:
EcoStruxure Operator Terminal Expert, Harmony HMIST6
Resolution:
When defining any username and password in your EcoStruxure Operator Terminal application, it is important to download the application either by USB Cable or Ethernet. During download, remember to choose the option to "Overwrite System Settings" to ensure that the security information is added/overwritten properly. When installing via VML file, these settings are retained and not overwritten.
Released for: Schneider Electric Global