Issue
Where do files with the file extension .HMIX come from?
Product Line
Vijeo Designer
Intelligent Data Services
Environment
HMI Configuration Software
Resolution
.HMIX extension files are exported from Vijeo Designer HMI applications that are used to create solutions for an add-on called Intelligent Data Services (IDS). IDS is a tool that runs on a Windows Server that is used to comply with FDA Electronic Records and Electronic Signatures standard "CFR 21 Part 11". for the Food and Pharmaceuticals industry.
To perform this export:
1) Right-click on the name of the HMI ("Target1" is the default name)
2) Choose "Export..." from the context menu

A Validation of the project will occur.
3) Save the file:

Where do files with the file extension .HMIX come from?
Product Line
Vijeo Designer
Intelligent Data Services
Environment
HMI Configuration Software
Resolution
.HMIX extension files are exported from Vijeo Designer HMI applications that are used to create solutions for an add-on called Intelligent Data Services (IDS). IDS is a tool that runs on a Windows Server that is used to comply with FDA Electronic Records and Electronic Signatures standard "CFR 21 Part 11". for the Food and Pharmaceuticals industry.
To perform this export:
1) Right-click on the name of the HMI ("Target1" is the default name)
2) Choose "Export..." from the context menu
A Validation of the project will occur.
3) Save the file:
Released for:Schneider Electric Global