{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do I log Time stamping events of the BMXERT1604T module via the OFS server?

Issue:
logging Time stamping events of the BMXERT1604T module via the OFS server


Product Line:
OFS Server, EcoStruxure Control Expert, BMXERT1604T


Resolution:
Below are the steps to configure Control Expert and the OFS server.
1. Ensure that Control Expert "Time Stamping Mode" is set to "System"
Control Expert

2. In this example, I will log channel 0 and 1 discrete value
CE

3. In the OFS configuration tool, I will leave the Timestamp group name to the default as shown. This name we will use for the group name for the testing client.
ce

4. Ensure that the Time Stamped Events service is checked. You can change polling rate for the ERT accordingly. It is left at default
ofs

5. Create a directory and then create a text file in that directory. The events will log to this file. In this example, the directory is called EVENT_LOG and the file name is ERT.txt
ofs1

6. Rick click on the shortcut for the OFS testing client and modify the Target. Add the following at the end of the string
-l C:\EVENT_LOG\ERT.TXT  as shown. So the full string should be
"C:\Program Files (x86)\Schneider Electric\OFS\Samples\OFSClient\ofsclient.exe" -l C:\EVENT_LOG\ERT.TXT
image6


7. When creating the group, give it the name ##TSEventsGroup##
image7

8. As you can see, the two variables are updated in the event group.
image8

9.  As shown, the events are being logged to the file
image9

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: