Issue: To what standard are the lifting devices designed and what is the weight limit?
Product Line: Circuit Breakers
Environment: Masterpact lifting devices S48900, S48901, S48906
Resolution:
The lifting devices are designed according to ASME B30.20 standards and structural design criteria per ASME BTH-1 design category B, service class 2.
Product Line: Circuit Breakers
Environment: Masterpact lifting devices S48900, S48901, S48906
Resolution:
The lifting devices are designed according to ASME B30.20 standards and structural design criteria per ASME BTH-1 design category B, service class 2.
The crossbars S48900 and S48901 have a maximum capacity of 500 pounds.
The lifting hooks S48906 have a maximum capacity of 165 pounds each.
Released for:Schneider Electric Global