SchneiderElectric_KBA_Basic_Meter_PM55xx Russian Language files issue
Problem statement :
Pm5560 Meter set to Russian language, the Panel data is not visible and some of data labels are not visible in different screen navigations.

Causes identified :
Solution :
Problem statement :
Pm5560 Meter set to Russian language, the Panel data is not visible and some of data labels are not visible in different screen navigations.
Causes identified :
- This data label missing or data missing in PM55xx is identified when Meter is set to Russian language.
- This is due to some issue with the Russian language file used within PM55xx.
- This issue is noticed with Pm55xx with firmware versions below 4.1.3
Solution :
- This issue is fixed in Firmware version 4.1.3 on wards. So meter needs to be upgraded to this Firmware version.
- Link for downloading the firmware : https://www.se.com/in/en/download/document/PM5560_PM5563_PM5580_V4.1.3/
Released for:Schneider Electric Global