{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can you setup the ATV320 Drive over Ethernet IP using assemblies 20 and 70?

Issue:

ATV320 using assemblies 20 and 70 with Ethernet IP

Product Line:

ATV320 with Ethernet TCP/IP option card part number VW3A3616.

Environment:

All

Cause:

Setting up Ethernet IP using assemblies 20 and 70.

Resolution:

Suggest you use Somove and ATV320 DTM file to configure the ATV320 drive

https://www.se.com/us/en/product-range/2714-somove/#software-and-firmware

PLC example setup:

Build a Generic Ethernet module configuration on the PLC side. Choose assemblies 20 and 70 for 2 words each.

20: Basic speed control output, size 2 words / 8 bytes

70: Basic speed control input, size 2 words / 8 bytes

The EtherNet/IP card translates the commands, behavior and monitoring information from of ODVA profile (on

the network) to the CiA402 profile (in the drive).

phot 1

phot 2

Phot 3

Setting up and programming the drive using Somove Software Example only.

Setting up the IP, subnet and gateway address

phot 4

Programming the drive per case II example in the Programming manual

phot 5

Commanding the drive to start, reset fault and speed control

1st word in the output table is the command word bit 0 =1 is run and bit 2 is fault reset

2nd word in the output table is the speed ref in rpms.

Reading Status from the drive like running, fault and motor speed.

1st word in the input table is the ETA Status word bit 0= fault and bit 2= Drive running

2nd word in the input table is the motor speed in rpms