{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can I use a generic SD card with the HMIG3U HMI?
Issue:
Using a generic SD card with the HMIG3U HMI


Product Line:
HMIG3U, Vijeo Designer


Resolution:
You may use any generic SD memory card up to 32Gig formatted for FAT32. There are different speed class. No particular speed class is required, however the higher the class number the faster the speed. Class 10 is recommended for better performance.

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: