{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why is the "œ" character not displayed correctly during EcoStruxure Operator Terminal Expert runtime?

Issue:
Character "œ" appears incorrectly during Runtime

Product Line:
EcoStruxure Operator Terminal Expert, Harmony HMI,

Resolution:
The language fonts on EcoStruxure Operator Terminal Expert are regulated by ISO standards.

The French_Gothic font set uses the character code [ISO IEC8859-1]. The "œ" character can not be displayed because it is a character that does not exist in the [ISO IEC 8859-1] character code.

Instead, use the Romanian_Gothic font set. This uses the character code [ISO IEC8859-16] which includes the "œ" character.

Schneider Electric Global

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: