{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Are fused switches available for the CF12KF63A36 OEM interior?

Issue:

Customer wants fused switches for the CF12KF63A36 OEM interior

Product Line:

QED2 OEM interiors

Environment:

CF12KF63A36

Cause:

Wants fused switch

Resolution:

No. The CF12KF63A36 is an I-line interior that will accept only I-line circuit breakers up to 250A. No fused switches are made for I-line interiors.

Schneider Electric Global