{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Difference on the reports produced by the DTM Audit Tool between a STA and STU file of the same application

Issue:
From CE 15.0, we note a malfunction on the registration of the file which deals with the DTM audit and which is the source of the problem related to the reliability of the DTM audit on a STA file? After a rebuild all of the project, this file which is in charge of the DTM audit is saved in two different locations, in the application archive file. On one of the locations, the file is not updated after a rebuild all of the project but on the other hand in this second location the update is done well. This results in the existence of a delta between the two records that are supposed to be the same. And this is the origin of the difference found by the DTM Audit tool on the DTM versions of the project between the STU file and the STA file of the same application. This case always appears if the application is native with a version less recent than the version with which we want to open the STA and STU files resulting from a total regeneration. For the STU file, the DTM audit does not report any problem, all the checkmarks are in green, on the other hand for the STA the Backwards compatibility box for certain equipment DTMs is in red.

Product Line :
From Control Expert v15.0

Resolution :
The issue was fixed and the fix will be published in Control-Expert V15.3.