{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Do we have the expected time difference between the operation of the early make N/O contact on a ZBE201 and the standard N/O Contact on the ZBE101?

Actually, the ZBE*** contact blocks are slow break action that means they are dependent of the head fitted with.

For example, if the customer is using a standard pushbutton, as a ZB4BA*, the speed of actuation of the contact block is directly linked to the speed actuation of the head.

At the opposite, if the customer is using an e-stop, which is a trigger action product like a snap action actuator, the contact block will be actually like that, i.e. closed to a simultaneous actuating.

Schneider Electric Global

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: