{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What replaces the LC breaker in an I-line interior?

Issue:

Needs to replace a LC breaker in an I-line interior

Product Line:

I-line circuit breaker

Environment:

Legacy LC frame

Cause:

LC Obsolete

Resolution:

The MJA breaker replaces the LC, however the MJA requires 9" of space where the LC only used 7.5", so they would need an additional 1-1/2" of mounting space in the I-line section per breaker.

Schneider Electric Global

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: