{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the BMKC8020310 High Speed counter A & B inputs can be used as standard inputs?
The signal InA and InB of each High Speed Channel can be used as discrete digital input with these restrictions:
The GND_SEN must be connected to 0Vdc and the 24v_SEN must be connected to the 24VDC to polarize each channel.

MC80 requirement

Schneider Electric Global

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: