{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Schneider Electric recommends using HTTPS instead of HTTP when accessing NetBotz version 3 appliances.
Issue:
Schneider Electric recommends using HTTPS instead of HTTP when accessing NetBotz version 3 appliances.

Product Line:
NetBotz

Environment:
NetBotz version 3
3.x and 4.x firmware

Cause:
HTTP is not a secure connection.

Resolution:
When accessing NetBotz version 3 (3.x and 4.x firmware) appliances, it is recommended that you use the most secure protocols available whenever possible. HTTPS is more secure than HTTP and should be used for either web connection or Advanced View connection.